Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerSCADA Operation (PSE/PSO) Alarm Filter Tree not appearing in runtime
Issue
When opening the Alarms page within the PSE runtime, the Alarm Filter Tree on the left side is blank and does not populate with the expected groups.

Product Line
PSE 8.1, 8.2
PSO 9.2

Environment
Runtime

Cause
The Report Server is what builds the Alarm Filter Tree.

Resolution
Add a Report Server to the PSE/PSO project and re-compile. Navigate away and back to the Alarm page and the Alarm Filter Tree should populate. Restarting project runtime is not required.