Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How long can be unshielded cables with IEC60034-25 motorsif ATV630/930 is used?
If the motor fullfil IEC60034-25, unshielded motor cables can be up to 150m without additional filter.