Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
IEC or EN60204-1 compatibility for ATV600/630?
IEC 60204-1: is standard for Safety of machinery - Electrical equipment of machines – Part 1: General requirements. This gives the stop category of safety function.

On ATV630 there is STO function This safety function corresponds to an uncontrolled stop in accordance with stop category 0 of IEC 60204-1.