Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the communication protocols supported by the power meter PM5560 with the reference METSEPM5560 ?
The communication protocols supported by the power meter PM5560 with the reference METSEPM5560 are as follows:

Modbus RTU and ASCII 2 wires with RS485 port, : 9.6, 19.2 and 38.4 kbauds, even/odd or none, insulation: 2500 V, JBUS
Modbus TCP/IP : 10/100 Mbit/s, insulation: 2500 V
Ethernet Modbus TCP/IP daisy chain with Ethernet port
BACnet IP

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre