Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to add an alarm for Digital I/O with a delay in PME.

Issue
PowerLogic devices with digital I/O alarms do not have the ability to add delays.

Product Line

Power Monitoring Expert (PME) 8.X
Power Monitoring Expert (PME) 9.x
Power Monitoring Expert (PME) 2020
Power Monitoring Expert (PME) 2021
Power Monitoring Expert (PME) 2022
Power Monitoring Expert (PME) 2023
Power Monitoring Expert (PME) 2024


Cause
PowerLogic devices such as CM4000 and PM800 devices have the ability to alarm on digital input status changes. Unfortunately there is no way to program a delay into the logic.

Resolution
With PME 8 and later version with alarm configuration we now have the ability to add delays to digital alarms. Adding a delay would make the alarms more consistent with other alarms that have delays built into them.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre