Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Data Quality Module (VEE) for PME/PSE?
Issue
What is the Data Quality Module (VEE) used for in PME/PSE

Product Line
Data Quality Module (VEE)

Environment
Power Monitoring Expert 8.1 or later
PowerSCADA Expert 8.1 or later

Cause
Analytics and entry of energy data as a result of datagaps within a database, meter rollover, resets and jitters.

Resolution
The Data Quality add-on module for StruxureWare power management platforms provides fully integrated Validation, Estimation and Editing (also known as VEE) that allows full quality control of logged system data.



Features:
• Interpolation of missing interval and cumulative data
• Identification of data gaps
• Identification of rollovers and resets
• Provide Automatic Analysis and Recommendations
• Color key indicators to quickly identify pertinent data
• Zoom-and-pan feature for closer inspection of data
• Security-locked to limit data correction and log access to Administrators
• Detailed data logs to audit track data corrections
• Rollback of modified data with a click

Able to be quoted/ordered in Stratus: 9789PMEDQM

Schneider Electric Saudi Arabia

Attachment(s)
4.14 Data Quality Module.pptx [1.53 MB]
Data Quality Module Print.pdf [429.56 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: