Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use PTC probe connected to encoder input on ATV340 (without encoder)?
It is possible. Encoder has to be configured to something, but usage of encoder has to be set to none. If it is set, encoder thermal monitoring can be activated and it will work.