Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What driver to use in Vijeo Designer to communicate to Allen Bradley Drive over Ethernet/IP?
Issue:
What driver to use in Vijeo Designer to communicate to Allen Bradley Drive over Ethernet/IP?

Product Line:
EIP, Magelis

Resolution:
Due to Vijeo Designer Rockwell EIP driver are specific to a controller type.  It is not possible to use that driver.  To communicate to any third party devices (including a AB drive) over Ethernet/IP, it is recommended to use the Ethernet/IP Explicit driver under Generic Drivers.