Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which version of wonderware client/drive will be compatible with OFS V3.6
Question:
Which version of wonderware client/drive will be compatible with OFS V3.6?

Answer:
Regarding compatibility, there is not known  issue of OFS regarding OPC DA 2.04 compatibility
If Wonderware Client/Drive is also compatible with  OPC DA 2.04, the compatibility with OFS should be ok