{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PowerChute Network Shutdown v4.2 not communicating with iReasoning or MG-Soft when authentication protocol is set to SHA 512.
Issue:
PowerChute Network Shutdown v4.2 not communicating with iReasoning or MG-Soft when authentication protocol is set to SHA 512

Product Line:
PowerChute Network Shutdown version 4.2

Environment:
PowerChute Network Shutdown version 4.2 configured with NMS tool iReasoning or MG-Soft

Cause:
SNMPv3  profile created with SHA 512

Solution:
Create profile with SHA 256

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.