Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Analog Output power supply be deactivated to connect to an externally powered monitor device on altivar process drive?
Issue:
Can the Analog Output power supply be deactivated to connect to an externally powered monitor device on altivar process drive?

Product line:
Altivar Process, ATV600 ATV900

Environment:
All

Cause:
Needs to use an external power supply

Resolution:
The Altivar Process drives do not have a means to deactivate the power supply on the AQ1 or AQ2 terminals.  The customer will need to find an external device to convert the signal.