Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the maximum value of energy for PM3200 series meters?

Issue

What are the maximum values of energy for PM3200 series meters?

Product Line

PowerLogic PM3200 Series

Environment

PM3200 Series Energy Meters – Energy Measurement Limits

Resolution

The energy values on PM3200 series meters automatically reset to 0 when they reach the following limits:

  • 1 × 10⁶ MWh (Active Energy)
  • 1 × 10⁶ MVAh (Apparent Energy)
  • 1 × 10⁶ MVARh (Reactive Energy)