Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
S765RDPS (ION7650 Remote Display) 24 Volt Power Supply Documentation

Issue:
User would like documentation, including drawings, of the 24VDC (PN: STEP-PS/ 1AC/24DC/0.75 - 2868635) power supply that is included with the M765RDPS

Product Line:
ION 7650 Remote Display

Environment:
DC Power Supplies

Cause:
The 24VDC power supply included with the S765RDPS is a third-party device that is manufactured by Phoenix Contact.

Resolution:
Please see the attached file for documentation on the TEP-PS/ 1AC/24DC/0.75 - 2868635 24VDC power supply. The Document is a user guide that includes specifications as well as drawings of the device.


Schneider Electric Saudi Arabia

Attachment(s)
24VPowerSupplyS765RDPS.pdf [311.73 KB]