Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is the MTZ firmware upgrade recommendation for 1.0.202 not shown in Ecoreach v2.5 if the Masterpact MTZ Micrologic module has a lower version installed?
Issue
The recommendation to do the firmware upgrade of the Masterpact MTZ Micrologic module is linked to the connection.  When connected through an Ethernet channel, Ecoreach v2.5  will show the Masterpact MTZ module firmware version.

Resolution
To check for new firmware and execute the update, a connection via USB must be done.  In Ecoreach 2.5, the Masterpact MTZ Micrologic module firmware upgrade requires a connection via the USB channel.