Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use network braking unit for Altivar ATV930 ?

Yes, there is new range of network braking units ATVRU75N4 (7.5kW unit) and ATVRD15N4 (15kW unit).
It is possible to combine up to 3 units in parallel. ATVR is compatible with Altivars: ATV320, ATV340 and ATV900.
Manual (NVE88423) and sizing tool (NVE94856) can be downloaded from schneider web.