Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to check PME web application's CPU and Memory usage using IIS

Issue
The memory usage of web application components is needed to troubleshoot high memory use or to optimize performance

Product Line

Power Monitoring Expert 2024

Power Monitoring Expert 2023

Power Monitoring Expert 2022

Power Monitoring Expert 2021

Power Monitoring Expert 9.x

Power Monitoring Expert 8.x

Power Monitoring Expert 7.2.x

Environment

Power Management Operations

Cause

Customer would like to investigate the current usage of the PME web applications


Resolution
Internet Information Services (IIS) Manager contains a feature called Worker Processes that can be used to monitor the memory and CPU usage on the server.

1- Make sure that PME's Web Applications is already open in any supported browser.
2- Open IIS manager. That can be done by running "inetmgr" command or by searching "IIS" in the search bar. (It is recommended to run as an admin.)
3- Click on the server name.
4- Double-click on Worker Processes as shown in the picture below.
Worker Processes location
5- The worker processes will list all the Application pools in use.
Worker Processes App Pools
Private Memory (Committed bytes) corresponds to actual RAM usage