Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What needs to be done to the ATV320 drive if you are using a ungrounded IT system?

Article available in these languages: Spanish

Issue:
ATV320 needs to use unground IT systems

Product Line:
Altivar Machines, Altivar 320

Environment:
All models and serial numbers

Cause:
IT ungrounded system

Resolution:
See the attached document IT grounding ground screw removal.pdf for the 230V drives, 400/460V B version drives and 400/460V C  version drives 4.0 kW and smaller.
For ATV320U55N4C - ATV320D15N4C see attached document IT_Jumper_ATV320_N4C.pdf

Schneider Electric Saudi Arabia

Attachment(s)
IT grounding ground screw disable.pdf [942.97 KB]
IT Jumper_ ATV320_N4C.pdf [315.15 KB]