Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the SSP04EMA series SPDs be used on a single phase 480V service?
The SSP04EMA series of SPDs are designed for 480/277Y three phase power. The SSP04 series of SPDs are not approved for application to a 480V single phase electrical system

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: