Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the CAN J1939 Protocol supported by SoMachine 4.3?
CAN J1939 Protocol is supported by SoMachine 4.3 This function and its documentation are delivered as a separated add-on to be installed on top of SoMachine V4.3. Refer to the Offer Manager or level 3 customer support to get this add-on.
- Availability on platforms: Modicon M241, M251
Note that Modicon M241 &M251 PLCs are not rugged certified against humidity and dust and may not be suitable to harsh environment
- License: No extra license required

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)