PlantStruxure PES [V4.2]: Dealing with unresponsive Genies above AN 9999 in PES 4.1 and PES 4.2.
Goals and Symptoms
How to correct the Genies inside PES Vijeo Citect having Animation Number more than 9999 which will not respond for any action during Citect runtime.
Causes and Fixes
The attached document illustrates the available methods to correct unresponsive Genie issue.The procedurre details to correct this issue using Citect patches inside PES VM. The patch replaces citect.frm inside VM Citect to accept the AN's more tha 9999.Released for: Schneider Electric Saudi Arabia