Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why, while configuring an IO module via the Dual Setting (Configure > Protection), does Ecoreach change the parameters for Inputs 5 and 6 of the IO module? (Configure > IO Config)
Issue:  While configuring an IO module via the Dual Setting (Configure > Protection) through Ecoreach the parameters inputs 5 and 6 of IO module are also changed.

Product Line: IO module, Ecoreach.

Cause:  Every time that user changes the configuration of an IO module and Control Unit, Ecoreach modifies the Inputs 5 and 6 of the IO module to ensure maximum coherence and security.

Resolution: ​After configuring the Dual Setting, check that the Inputs 5 and 6 of the IO module are configured properly. If not, configure them as required and click Write to Device.