Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are installation possibilities of (ceiling) Argus detectors?
1) installation in flush-mounted boxes with screw fixing (60 mm)
2) surface-mounted housing (art. no.: MTN550619) 105 x 36 mm

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: