Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement connector (2 positions) of the TSXASY800 card?
Issue:
We need to order a replacement connector for the 2 positions green connector of the TSXASY800 premium card.

Product Line:
Premium, TSX, Modicon

Environment:
PLC

Resolution:
The connector on the TSXASY800 is not sold separate, we do not have a part number for it. However the customer can obtain the connector through Phoenix Contact. The manufacturer part number is 1757019. The part number alias is MSTB_2,5.

Schneider Electric Saudi Arabia

Attachment(s)
1757019.pdf [230.88 KB]