Search FAQs
What is the UL Type 1 Conformity Kit for the ATV630 High HP drives?
Issue:
Selection for UL Type 1 Conformity Kit from the ATV630 catalog. The catalog lists two options.
VW3A9212
VW3A9213 (without brake resistor)
Product line:
Altivar 630, ATV630
ATV630C22N4
ATV630C25N4
ATV630C31N4
Environment:
models listed
Cause:
Catalog error
Resolution:
The ATV630 drive cannot use Brake resistors. So the only available Type 1 Conformity kit is VW3A9213.
Selection for UL Type 1 Conformity Kit from the ATV630 catalog. The catalog lists two options.
VW3A9212
VW3A9213 (without brake resistor)
Product line:
Altivar 630, ATV630
ATV630C22N4
ATV630C25N4
ATV630C31N4
Environment:
models listed
Cause:
Catalog error
Resolution:
The ATV630 drive cannot use Brake resistors. So the only available Type 1 Conformity kit is VW3A9213.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: