Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the IEM3255 be monitored remotely via WiFi?

Issue:
Can the IEM3255 communicate via WIFI?

Product:
IEM3255

Environment:
Ethernet Communications / Wireless Communications

Resolution:
Unfortunately, not. The IEM3255 is only capable of Modbus RTU. However, the meter can utilize one of our ethernet gateways such as the PAS600L which will allow for a WIFI router to connect to it. For information on the PAS600 please click here. To view information on how to configure an Ethernet Gateway check out the FAQ FA239552

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: