Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can historical data be transferred automatically from ION6 to Power Manager 1.3?
The historical data cannot be transferred automatically, but must be done manually which is a lengthy process.

This is done using SQL database.

It cannot be done using something like ETL as ETL is only to be used between Schneider Electric software.

Please see email explaining that the historical data must be transferred using SQL database.

If the historical data is needed a suggestion it to upgrade to the latest version PME, 8.2, as the historical data with be transferred automatically.




Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre