Issue:
ATV320 auto manual control set up.
Product Line:
Altivar 320
Environment:
Applies to all ATV320 drives
Cause:
Wants to set up an 3 position switch for HOA control.
Resolution:
To program the drive for auto manual/hand control follow the below steps
Go to Conf -> FULL -> CTL-
1. Set Fr1 = the speed channel in manual/hand mode
3. Set CCS = LIx (replace x with the number of the input you want to use to switch between hand and auto)
4. Set CD1 = the command channel in manual/hand mode where will the start/stop command come from
6. Set RFC = LIx (replace x with the number of the input you want to use to switch between hand and auto)
7. Set FR2 = the speed channel in auto mode (see list above same as FR1, for full description refer to the programming manual)
See the ATV320 Programming Manual for further details.
ATV320 auto manual control set up.
Product Line:
Altivar 320
Environment:
Applies to all ATV320 drives
Cause:
Wants to set up an 3 position switch for HOA control.
Resolution:
To program the drive for auto manual/hand control follow the below steps
Go to Conf -> FULL -> CTL-
1. Set Fr1 = the speed channel in manual/hand mode
Options:
AI1 = 0-10V signal
AI2 = -10 +10V signal
AI3 = 0 - 20mA or 4 - 20mA signal
AIUI = the virtual pot on the drive itself
LCC = speed from the remote display
MDB = speed over modbus communication
CAN = speed over CanOpen communication
NET = speed over the communication card inserted (Ethernet IP, modbus TCP, etc..)
2. Set CHCF = SEP (separate controls) Hold Enter for 2 seconds to make this changeAI1 = 0-10V signal
AI2 = -10 +10V signal
AI3 = 0 - 20mA or 4 - 20mA signal
AIUI = the virtual pot on the drive itself
LCC = speed from the remote display
MDB = speed over modbus communication
CAN = speed over CanOpen communication
NET = speed over the communication card inserted (Ethernet IP, modbus TCP, etc..)
3. Set CCS = LIx (replace x with the number of the input you want to use to switch between hand and auto)
4. Set CD1 = the command channel in manual/hand mode where will the start/stop command come from
Options:
TER = start stop on the digital inputs of the drive
LCC = start stop from the remote keypad
MDB = command over modbus communication
CAN = command over CanOpen communication
NET = command over the communication card inserted
5. Set CD2 = the command channel in the auto mode (same options as above)TER = start stop on the digital inputs of the drive
LCC = start stop from the remote keypad
MDB = command over modbus communication
CAN = command over CanOpen communication
NET = command over the communication card inserted
6. Set RFC = LIx (replace x with the number of the input you want to use to switch between hand and auto)
7. Set FR2 = the speed channel in auto mode (see list above same as FR1, for full description refer to the programming manual)
See the ATV320 Programming Manual for further details.
Released for: Schneider Electric Saudi Arabia