Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why am I unable to perform the Automatic Trip Curve Test for earth leakage protection using Ecoreach on Masterpact MTZ Micrologic 7.0X?
Issue: It is not possible to perform the Active Trip Curve Test for Earth Leakage protection using Ecoreach.
Cause: The Dual Setting is not enabled from the Micrologic X HMI and the Set B is set to active. To perform the Active Trip Curve Test for Earth Leakage protection using Ecoreach switch set A to be active using Ecoreach.