Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Execution sequence (Scan order) of FBD section in Unity Pro

Issue:
In which order are the function blocks scanned (or execution sequence) in a Unity Pro FBD section?

Product Line:
Programming software

Environment:
Unity Pro

Cause:

Resolution:
The blocks are scanned (or executed) in the following order:
From top left position to bottom right position, with top having priority over left, as shown below (case 1)

img1

If blocks are linked together, the execution order will now follow the flow of the link (case 2)

img2

You can also force the execution sequence by going in the properties of the function block (case 3)

img3

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)