Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
B10d calculation for normally closed contact ZBE102 ?
FOR NORMALLY CLOSED CONTACT (ZBE102)
The fault exclusion described in Table D8 from ISO 13849-2 2012 can be considered
As our contact ZBE102 respects requirements and verification test according to the IEC 60947-5-1:2003 Annex K “Special requirements for control switches with direct opening action”, so the B10d cannot have to be considered thanks to the exclusion fault.

Schneider Electric Saudi Arabia

Attachment(s)
17-017 C&S B10d for ZBE102.pdf [218.36 KB]
ISO 13849-2 2012 Table D8.docx [150.26 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: