Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you configure ION Meters to accept multiple 61850 clients?

Issue

The user would like to configure ION Meters to accept multiple 61850 clients

Product Line

ION Meters

Environment

Meter protocol configuration

Cause

The user want to connect multiple 61850 Clients on a single ION meter.

Resolution

There are no settings that you can change in your ION Meter regarding number of accepted Client connections.

That is hardcoded in the meter's firmware, no matter which communication protocol is used to connect to the meter.