Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert Diagnostic File Error


Issue:
After running the Diagnostic Tool, a .CAB file is never created.

Product:
Power Monitoring Expert 2024

Power Monitoring Expert 2023

Power Monitoring Expert 2022

Power Monitoring Expert 2021

Power Monitoring Expert 2020

Power Monitoring Expert 9.0

Power Monitoring Expert 8.x

Power Monitoring Expert 7.2


Environment:
Power Monitoring Software

Resolution:
There are 2 possible solutions below.

  1. A workaround would be unchecking the check box "Compress Package" in the tool so that you will get the diagnostic folder contains all the info.
  2. Inside the PME installer file, there is 'DiagnosticsTool_x86.exe' under the folder \setup\Installers. You can use this to reinstall the tool.

If you do not have the installation file, you may download the installation files from our website. Please check what version you are running before using the installation file.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: