Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use Modbus port for Modbus RTU communication and Graphical panel VW3A1111 for ATV320 drives?
On ATV320, VW3A1111 (or any display via modbus serial) and modus RTU communication cannot be used at the same time.