Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to check I/O Memory consumption in EcoStruxure Control Expert ?
In EcoStruxure Control Expert, you can monitor the I/O memory consumption by viewing the bus properties.
Use one of these methods:
  • In the Project Browser, right-click Project → Configuration → EIO Bus → Properties
  • In the Project Browser, right-click Project → Configuration → EIO [Quantum or Modicon X80] Drop → Properties
  • In the background of the EIO Bus window, right-click Bus properties
  • In the Edit menu, select Bus properties.