Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the USB programming cable that can be used with serial RJ-45 or Sub-D 9 Pin port of Quantum PLC ?

Here is a list of combination cables to connect Quantum PLC over USB :

  • Quantum High End with serial RJ45 Quantum use TSXCUSBRS232 + ( 110XCA28202  OR 110XCA20300 )
  • Quantum Low End with seriab SUB D 9 connector use TSXCUSBRS232  +  990NAA26320

    Quantum Cables