Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the list of drivers supported with Vijeo XD 2016 SP2 (SW v2.4.2) ?
Here is list of  Drivers Supported PLCs  with Vijeo XD 2016 SP2 (SW v2.4.2)

Schneider Electric SA
- MODBUS TCP Master
- MODBUS TCP Master USB Equipment
- MODBUS SIO Master
- MODBUS SIO Master CT Equipment
- Uni-Telway
- PacDrive Ethernet Cx00 - (Codesys V3.5)
- PacDrive Ethernet LMC x00C - (Codesys V3.5)
- MODBUS TCP Slave
- MODBUS SIO Slave
- MODBUS SIO ASCII Master
- SoMachine Network
- Zelio Logic

Mitsubishi Electric Corporation
- Q/QnA Series Ethernet
- Q Series CPU Direct
- Q/QnA Series Serial
- FX Series CPU Direct
- FX Series Ethernet
- FX Series Computer Link
- Q Series QnU CPU Ethernet
- iQ-R/F Series Ethernet

Rockwell Automation
- EtherNet/IP (Symbol sharing with RSLogix 5000)
- DF1
- DH-485

Siemens AG
- SIMATIC S7 MPI Direct
- SIMATIC S7 MPI Direct - 12M (CoPla*)
- SIMATIC S7 Ethernet (LOGO!8 support)

OMRON Corporation
- CS/CJ Series HOST Link
- CS/CJ Series Ethernet
- CS/CJ/NJ Series EtherNet/IP (Symbol sharing with Sysmac Studio)

Emerson Process Management
- ROC Plus SIO
- ROC Plus Ethernet

CAN in Automation
- CANopen Slave (CoPla*)

PROFIBUS International
- PROFIBUS DP Slave (CoPla*)

* CoPla units are NOT available