How can we help you today?

How many alarms can display on alarm viewer in M580 web server?

the alarm viewer is the same as the diagnostic viewer in Unity, the message number is depending on the diagnostic buffer in CPU (4Kb-8Kb according to different CPU types).
When the diagnostic buffer is full, the new alarm will not be written. %S77 indicating if the buffer is full or not.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation