Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What's the basic or typical combination of XVU range?
The basic or typical combination of XVU range as below:
Without Buzzer: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + LED lights (XVUC23~XVUC29)
With Buzzer: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + LED lights (XVUC23~XVUC29) + XVUC9S(x)
With Sound: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + Sound unit (XVUC9V) + LED lights (XVUC23~XVUC29)
With PWM units: Base unit (XVUZ0x) + AC body or DC body (XVUC21x) + XVUC9VP and / or XVUC29VP