Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If a drive is set for 3-wire control, can it be switched internally by the drive to 2-wire control?
Issue:
Configuration modification from 3 to 2-wire control

Product Line:
Altivar Drives

Environment:
ATV312, ATV212, ATV61, ATV71, ATV630, ATV930, ATV320,

Cause:
Customer application requirement

Resolution:
No, the drive is not capable of switching 3-wire to 2-wire control internally.