Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Conditional rated short circuit current (Inc/I∆c) , For RCCB-ID B type ?
The Conditional rated short circuit current :
25/40 A with FU 80 A gG fuse  ==>  10,000 A
63 A with FU 100 A gG fuse   ==>  10,000 A
80/125 A with FU 125 A gG fuse ==>  10,000 A