Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the way to register SFT2841 without connecting the PC to the network or to the internet?
Due to security reasons, some PCs are not allowed to be connected to the internet or network and not allowed to have connection with foreign USB dongle or USB stick. If this is the case, the only option to register SFT2841 is by using the “register by phone” option.

Below are the call center numbers.
  • USA: +1 888 266 8705 from US and Canada - English - 8:00am to 5:00pm (EST**) or +1 978 975 9755 from other countries - English - 8:00am to 5:00pm (EST**)
  • Czech Republic: +420 281 088 696 - English - 8:30am to 5:00pm (CET*)
  • France: +33 (0) 492 08 82 68 - French/English/Spanish/Italian/German - 8:00am to 6:00pm (CET*)
The call centers are open during the stated hours, Monday to Friday only. *CET : Central European Time **EST : Eastern Standard Time

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: