Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV680- Do the input wires and motor wires come in the top or bottom?

Issue:
Do the input wires come from the top or from the bottom on ATV680

Product Line:
ATV680

Resolution:
According to the ATV680 Handbook (NHA37113) , the input power wiring and motor wiring come from the bottom of the enclosure.   To wire from the top, they will need a Q  option ( Door Mounted Overload Reset Push Button) & U option (Top Entry Cubical )

See page 95 of The ATV680 Handbook.

Schneider Electric Saudi Arabia

Attachment(s)
ATV680_Handbook_EN_NHA37113_02.pdf [7.46 MB]