{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the leakage current on the output of the ATV212 drive?

Article available in these languages: Japanese

Issue:
Leakage current on the output of the ATV212 drive

Product Line:
ATV212

Environment:
All

Cause:
Wants leakage below 1.1mA

Resolution:
The amount of leakage current is dependent on several factors.
Please refer to the ATV212 catalog (link HERE ) for specific details
If leakage needs to be below the listed values, an output contactor or other type of disconnect must be used to fully isolate the motor from the VFD output.

Schneider Electric Saudi Arabia