Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to power the ATV630 or ATV930 drive with an external +24VDC power supply?
Issue:
Is it possible to power the ATV630 or ATV930 drive with an external +24VDC power supply?

Product Line:
Variable Frequency Drives

Environment:
Applies to ATV630, ATV930

Cause:
Need to power the electronics of the drive from a separate external +24Vdc source in the panel

Resolution:
Yes, use an external 24Vdc power supply and wire it to "P24" and "0V" terminals on the ATV630 and ATV930.

Note: You cannot run a drive with only 24VDC provided. Use an external 24V only to power the electronics of the drive for programming purposes.