Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for door screws of the ATS48 Enclosed Soft Starert?
Issue:
Part number for door screws of ATS48 Enclosed Soft starter?

Product Line:
ATS48 enclosed

Environment:
All

Cause:
NA

Resolution:
The part number for the screw is 80450-350-50. This part number is an assembly of the 1/4 turn screw, retainer, receptacle and screw.