What does 383 on the end of the ATV71 part number indicate?
Issue:
Part number ending in 383
Product Line:
Altivar71
Environment:
ALL
Cause:
Special Firmware Requirement for Altivar 71
Resolution:
This was a special firmware version for use with Permanent Magnet Motors.
Current drives ATV600, ATV900, ATV320, ATV340 all have PM Motor parameters by default.
Part number ending in 383
Product Line:
Altivar71
Environment:
ALL
Cause:
Special Firmware Requirement for Altivar 71
Resolution:
This was a special firmware version for use with Permanent Magnet Motors.
Current drives ATV600, ATV900, ATV320, ATV340 all have PM Motor parameters by default.
Released for: Schneider Electric Saudi Arabia