How can we help you today?

Does the Bacnet card for ATV600 drive support star or ring topology?

Issue:
When the ATV600 is used on a Bacnet network, is a star or ring topology supported?

Product line:
ATV630, VW3A3725

Environment:
All models, All serial numbers.

Cause:
Bacnet Communications

Resolution:
No.  Bacnet should be connected in a daisy chain configuration only.

Schneider Electric Saudi Arabia