Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the specifications for the STO inputs, on the ATV Process drives?
Issue:
Looking for the specifications for the STO inputs, on the ATV Process drives?

Product Line:
Altivar Process Drives
ATV630
ATV930

Environment:
All

Cause:
STO inputs specifications

Resolution:
Characteristics of ATV Process STO inputs
PLC compatibility:  complies with IEC/EN61131-2 logic type 1 and type 3, for voltage levels
Positive logic (Source):
State 0 if  ≤ 5Vdc or STO not wired,
State 1 if ≥ 11Vdc
Impedance: ≥ 2.2kΩ
Maximum current:      10mA min at 19V input for external (Preventa) Relay
Response time: 10ms