Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the AQ1 max percent value on the ATV630 and ATV930 process drives when you are outputting mA's for motor current?
Issue:
AQ1 max percent value on the ATV630 and ATV930 when outputting mA's for motor current

Product Line:
Altivar ATV630 and ATV930 drive

Environment:
All

Cause:
100% means 2X the drives current IN ratings.

Resolution:
[Motor Current] OCr Current in the motor, from 0 to 2 In (In = rated drive current indicated in the
Installation manual and on the drive nameplate)

If you want to reduce the range down to 0 to 1 In just change the max percent down to 50%

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre