Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find the Profinet GSD file for the ATV600 and ATV900 drives?
Issue:
Where can I find the GSDML file for ProfiNet to use with the Altivar 630 or Altivar 930 drives?

Product Line:
Altivar 630 and 930

Environment:
All serial numbers for Altivar 630 and 930

Cause:
GSD file for profinet

Resolution:
https://www.se.com/ww/en/download/document/PROFINET_GSDML_VW3A3627/